1.4.3.24 PAL_GetTimerExtended Function
C
uint8_t PAL_GetTimerExtended(uint16_t pch, uint64_t *timer);
Summary
Get the extended PHY time in us.
Description
This routine is used to get the extended PHY time.
Precondition
The PAL_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| pch | Physical channel |
| timer | Extended output time of PHY |
Returns
PAL_CFG_SUCCESS - If successful
PAL_CFG_INVALID_INPUT - If unsuccessful
Example
uint8_t result=PAL_CFG_SUCCESS;
uint64_t timer=0;
uint16_t pch=1;
result = PAL_GetTimerExtended(pch, &timer);
Remarks
None.