1.4.3.22 PAL_GetZCT Function
C
uint8_t PAL_GetZCT(uint16_t pch, uint32_t *zct);
Summary
Get zero-cross time (ZCT).
Description
This function is used to get the value of the zero-cross time of the mains and the time between the last transmission or reception and the zero cross of the mains.
Precondition
The PAL_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| pch | Physical channel |
| zct | Zero time output parameter |
Returns
PAL_CFG_SUCCESS - If successful
PAL_CFG_INVALID_INPUT - If unsuccessful
Example
uint8_t result=PAL_CFG_SUCCESS;
uint8_t zct=0;
uint16_t pch=1;
result = PAL_GetZCT(pch, &zct);
Remarks
Not available for both PHY Serial and RF medium.