6.4.4 NVMREG Erase of Program Memory
Before writing to program memory, the word(s) to be written must be erased or
previously unwritten. Program memory can only be erased one row at a time. No automatic
erase occurs upon the initiation of the write to program memory. To erase a program
memory row:
- Clear the NVMREGS bit of the NVMCON1 register to erase program memory locations, or set the NMVREGS bit to erase User ID locations.
- Write the desired address into the NVMADRH:NVMADRL register pair.
- Set the FREE and WREN bits of the NVMCON1 register.
- Perform the unlock sequence as described in the “NVM Unlock Sequence” section.
If the program memory address is write-protected, the WR bit will be cleared and the erase operation will not take place.
While erasing program memory, CPU operation is suspended, and resumes when the operation is complete. Upon completion, the NVMIF is set, and an interrupt will occur if the NVMIE bit is also set.
Write latch data is not affected by erase operations, and WREN will remain unchanged.
Note: See the previous figure.
Erasing One Row of Program Flash Memory
; This sample row erase routine assumes the following: ; 1.A valid address within the erase row is loaded ; in variables ADDRH:ADDRL ; 2.ADDRH and ADDRL are located in common RAM ; (locations 0x70 - 0x7F) BANKSEL NVMADRL MOVF ADDRL,W ; Load lower 8 bits of MOVWF NVMADRL ; erase address boundary MOVF ADDRH,W ; Load upper 6 bits MOVWF NVMADRH ; of erase address boundary BCF NVMCON1,NVMREGS ; Choose PFM memory area BSF NVMCON1,FREE ; Specify an erase operation BSF NVMCON1,WREN ; Enable writes BCF INTCON,GIE ; Disable interrupts during ; unlock sequence ; ------------------REQUIRED UNLOCK SEQUENCE:----------------- MOVLW 0x55 ; Load 0x55 to get ready for ; unlock sequence MOVWF NVMCON2 ; First step, load 0x55 into NVMCON2 MOVLW 0xAA ; Second step, load 0xAA into W MOVWF NVMCON2 ; Third step, load 0xAA into NVMCON2 BSF NVMCON1,WR ; Final step, set WR bit ; -------------------ERASE IS COMPLETE---------------------- BSF INTCON,GIE ; Re-enable interrupts BCF NVMCON1,WREN ; Disable writes
| Host Values | NVMREG Access | FSR Access | ||||||
|---|---|---|---|---|---|---|---|---|
| Memory Function | Memory Type | Program Counter (PC) | ICSP™ Address | NVMREGS bit (NVMCON1) | NVMADR[14:0] | Allowed Operations | FSR Address | FSR Programming Access |
| RESET VECTOR | Program Flash Memory | 0x0000 | 0x0000 | 0 | 0x0000 | READ/WRITE | 0x8000 | READ ONLY |
| USER MEMORY | 0x0001 | 0x0001 | 0 | 0x0001 | 0x8001 | |||
| 0x0003 | 0x0003 | 0x0003 | 0x8003 | |||||
| INT VECTOR | 0x0004 | 0x0004 | 0 | 0x0004 | 0x8004 | |||
| USER MEMORY | 0x0005 | 0x0005 | 0 | 0x0005 | 0x8005 | |||
| 0x7FFF(1) | 0x7FFF(1) | 0x7FFF(1) | 0xFFFF | |||||
| USER ID | Program Flash Memory | NO PC ACCESS | 0x8000 | 1 | 0x0000 | READ/WRITE | NO ACCESS | |
| 0x8003 | 0x0003 | |||||||
| Reserved | — | — | — | 0x0004 | — | |||
| REV ID | HC | 0x8005 | 1 | 0x0005 | READ | |||
| DEVICE ID | 0x8006 | 1 | 0x0006 | |||||
| CONFIG1 | FUSE | 0x8007 | 1 | 0x0007 | READ/WRITE | |||
| CONFIG2 | 0x8008 | 1 | 0x0008 | |||||
| CONFIG3 | 0x8009 | 1 | 0x0009 | |||||
| CONFIG4 | 0x800A | 1 | 0x000A | |||||
| CONFIG5 | 0x800B | 1 | 0x000B | |||||
| DIA and DCI | PFM | 0x8100 | 1 | 0x0100 | READ | |||
| 0x82FF | 1 | 0x02FF | ||||||
| USER MEMORY | EEPROM | 0xF000 | 1 | 0x7000 | READ/WRITE | 0x7000 | READ ONLY | |
| 0xF0FF | 0x70FF | 0x70FF | ||||||
Note:
- The maximum Program Flash Memory address for the PIC16(L)F184XX family is 0x7FFF.