6.4.7 NVMREG Access to Device Information Area, Device Configuration Area, User ID, Device ID, EEPROM, and Configuration Words
NVMREGS can be used to access the following memory regions:
- Device Information Area (DIA)
- Device Configuration Information (DCI)
- User ID region
- Device ID and Revision ID
- Configuration Words
- EEPROM
The value of NVMREGS is set to ‘1’ in the NVMCON1 register
to access these regions. The memory regions listed above would be pointed to by PC[15] =
1, but not all addresses reference valid data. Different access may
exist for reads and writes. Refer to the table below. When read access is initiated on
an address outside the parameters listed in the following table, the NVMDATH: NVMDATL
register pair is cleared, reading back ‘0’s.
| Address | Function | Read Access | Write Access |
|---|---|---|---|
| 0x8000 - 0x8003 | User IDs | Yes | Yes |
| 0x8005 - 0x8006 | Device ID/Revision ID | Yes | No |
| 0x8007 - 0x800B | Configuration Words 1-5 | Yes | Yes |
| 0x8100 - 0x82FF | DIA and DCI | Yes | No |
| 0xF000 - 0xF0FF | EEPROM | Yes | Yes |
Device ID Access
; This write routine assumes the following: ; 1. A full row of data are loaded, starting at ; the address in DATA_ADDR ; 2. Each word of data to be written is made up of ; two adjacent bytes in DATA_ADDR, stored in little endian format ; 3. A valid starting address (the Least Significant bits = 00000) ; is loaded in ADDRH:ADDRL ; 4. ADDRH and ADDRL are located in common RAM (locations 0x70-0x7F) ; 5. NVM interrupts are not taken into account BANKSEL NVMADRH MOVF ADDRH,W MOVWF NVMADRH ; Load initial address MOVF ADDRL,W MOVWF NVMADRL MOVLW LOW DATA_ADDR ; Load initial data address MOVWF FSR0L MOVLW HIGH DATA_ADDR MOVWF FSR0H BCF NVMCON1,NVMREGS ; Set PFM as write location BSF NVMCON1,WREN ; Enable writes BSF NVMCON1,LWLO ; Load only write latches LOOP MOVIW FSR0++ MOVWF NVMDATL ; Load first data byte MOVIW FSR0++ MOVWF NVMDATH ; Load second data byte CALL UNLOCK_SEQ ; If not, go load latch INCF NVMADRL,F ; Increment address MOVF NVMADRL,W XORLW 0x1F ; Check if lower bits of address ; are 00000 ANDLW 0x1F ; and if on last of 32 addresses BTFSC STATUS,Z ; Last of 32 words? GOTO START_WRITE ; If so, write latches to memory GOTO LOOP START_WRITE BCF NVMCON1,LWLO ; Latch writes complete, ; Now write memory CALL UNLOCK_SEQ ; Perform required unlock sequence BCF NVMCON1,LWLO ; Disable writes UNLOCK_SEQ MOVLW 0x55 BCF INTCON,GIE ; Disable interrupts MOVWF NVMCON2 ; Begin unlock sequence MOVLW 0xAA MOVWF NVMCON2 BSF NVMCON1,WR BSF INTCON,GIE ; Re-enable interrupts ; Unlock sequence complete RETURN