6.3.2.3 Asynchronous Response Format
The ADC module generates asynchronous responses after each conversion. This value returned is an
instantaneous value upon receiving the AT command. The response format is as
follows:
+ADCRDVAL: <Value>, <Channel>- Value: This field represents the instantaneous digital value obtained from the analog-to-digital conversion. It can range from ‘0’ to the maximum value supported by the ADC resolution.
- Channel: This field indicates the channel number from which the conversion was performed. It can be one of the supported channels.