3.4 USB Connectivity using Microchip USB 2.0 Hub
Controller
The WBZ351 Curiosity Board has two USB end devices: PKOB4 and MCP2200.
Both these USB devices are accessible to the upstream PC via a common USB connector
using the Microchip USB 2.0 High Speed Hub Controller USB2512B providing the user with
more ease of use.Figure 3-3. USB Connectivity using Hub
Controller
After plugging the WBZ351 Curiosity Board into the upstream PC
using a micro USB cable, device enumeration is as shown in the following figure for the
PKOB4 and MCP2200.Figure 3-4. Device Manager