The following are the list of sources to power the WBZ351 Curiosity
Board:
A host PC can power the WBZ351 Curiosity Board over USB using a Type-A-to-Micro-B USB cable
connected to a Micro-B USB connector (J7).
4.2V Lithium battery (Li-ion/Li-Po) battery kit
as follows:
Connected to battery header
(J3), JST PH, 2-pin, 2 mm pitch and right-angle male
battery header
Crimp style connector,
battery polarity according to +/- marking on the board
Battery is not part of the
kit
Minimum recommended battery
capacity is 400 mAh with a battery charge voltage of 4.2V
Battery management circuit automatically handles selection between the USB power supply and
battery supply.
The following are the two on-board MCP1727 voltage regulators on the WBZ351 Curiosity Board that power the circuitry on-board.
Voltage regulator (U10) – Generates 3.3V that powers the WBZ351PE Module along with the associated
circuits
Voltage regulator (U13) – Generates 3.3V that powers the USB hub IC
(U201), PKOB4 main controller (U300), along with the associated circuits that
connect the PKOB4 debugger to a host PC and MCP2200 USB to UART converter
For more details on the U10 and U13 voltage regulators, refer to the MCP1727 1.5A, Low
Voltage, Low Quiescent Current LDO Regulator Data Sheet (DS21999).Figure 3-2. WBZ351 Curiosity Board Power
Supply Block Diagram
The WBZ351PE Module and associated peripherals can also be powered
from:
External power supply header (J5) using an external power supply (1.9-3.6V) for testing
at different voltage levels apart from the default supply of 3.3V from the on-board
regulator. To use the external power supply header, disconnect the on-board 3.3V
supply according to the following table:
Table 3-2. Jumper Option (J5) to Select the
WBZ351PE Module Power Supply
On-board 3.3V Regulator
External Power Supply
Short J5 pin 1 and pin 2, with shunt resistor (R36) mounted (default configuration)
Use J5 pin 2 for external power and J5 pin 3 for GND connection. Do
not mount R36.
Note: The maximum available current from the PC host USB is
limited to 500 mA. The current is shared between charging the external battery (if
connected) and the target application section.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.