1.4.3.14 SYS_WIFI_Deinitialize Function
C
SYS_WIFI_RESULT SYS_WIFI_Deinitialize (SYS_MODULE_OBJ object)
Summary
Deinitializes the module instance of the system Wi-Fi service
Description
This function deinitializes the module instance disabling its operation. Resets all of the internal data structures and fields to the default settings.
Precondition
The SYS_WIFI_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | SYS WIFI object handle, returned from SYS_WIFI_Initialize |
Returns
return SYS_WIFI_RESULT
Example
if (SYS_WIFI_SUCCESS == SYS_WIFI_Deinitialize (sysObj.syswifi))
{
// when the SYS WIFI is De-initialized.
}Remarks
Deinitialize should be called if the WiFi service is no longer going to be used.