1.4.3.16 SYS_WIFI_Initialize Function
C
SYS_MODULE_OBJ SYS_WIFI_Initialize ( SYS_WIFI_CONFIG *config, SYS_WIFI_CALLBACK callback, void *cookie )
Summary
Initializes the System Wi-Fi module.
Description
Wi-Fi service supports only one single instance of Wi-Fi.
Parameters
| Param | Description |
|---|---|
| config | Wi-Fi device configuration structure. |
| callback | The client callback function pointer. |
| cookie | The pointer which will be passed to the customer application when the customer callback function is invoked. |
Returns
If successful, returns a valid handle to an object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.
Example
#define WIFI_DEV_SSID "DEMO_AP" #define WIFI_DEV_PSK "password" SYS_WIFI_CONFIG wifiSrvcConfig; // Set mode as STA wifiSrvcConfig.mode = SYS_WIFI_STA; // Disable saving wifi configuration wifiSrvcConfig.saveConfig = false; // Set the auth type to SYS_WIFI_WPA2 wifiSrvcConfig.staConfig.authType = SYS_WIFI_WPA2; // Enable all the channels(0) wifiSrvcConfig.staConfig.channel = 0; // Device doesn't wait for user request wifiSrvcConfig.staConfig.autoConnect = 1; // Set SSID memcpy(wifiSrvcConfig.staConfig.ssid,WIFI_DEV_SSID,sizeof(WIFI_DEV_SSID)); // Set PSK memcpy(wifiSrvcConfig.staConfig.psk,WIFI_DEV_PSK,sizeof(WIFI_DEV_PSK)); sysObj.syswifi = SYS_WIFI_Initialize(&wifiSrvcConfig, WiFiServCallback, 0); if (sysObj.syswifi == SYS_MODULE_OBJ_INVALID) { // Handle error }
Remarks
This routine can only be called once during system initialization. If the Wi-Fi system service is enabled using MHC, then auto generated code will take care of system wi-fi initialization.