1.4.3.17 SYS_WIFI_Tasks Function
C
uint8_t SYS_WIFI_Tasks ( SYS_MODULE_OBJ object)
Summary
Maintains the Wi-Fi System tasks and functionalities.
Description
This function is used to run the various tasks and functionalities of Wi-Fi system service.
Precondition
The SYS_WIFI_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | SYS WIFI object handle, returned from SYS_WIFI_Initialize |
Returns
return SYS_WIFI_STATUS if client provided object is valid, else return SYS_WIFI_OBJ_INVALID.
Example
if (SYS_WIFI_OBJ_INVALID != SYS_WIFI_Tasks (sysObj.syswifi))
{
}
Remarks
If the Wi-Fi system service is enabled using MHC, then auto generated code will take care of system task execution.