1.5.3.12 SYS_WIFIPROV_GetStatus Function
C
uint8_t SYS_WIFIPROV_GetStatus ( SYS_MODULE_OBJ object)
Summary
Returns System Wi-Fi Provisioning service status.
Description
This function returns the current status of the System Wi-Fi Provisioning service.
Precondition
The SYS_WIFIPROV_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | SYS WIFIPROV object handle, returned from SYS_WIFIPROV_Initialize |
Returns
return SYS_WIFIPROV_STATUS if client provided object is valid, else return SYS_WIFIPROV_OBJ_INVALID.
Example
if (SYS_WIFIPROV_STATE_WAITFORREQ == SYS_WIFIPROV_GetStatus (wifiProvServHandle))
{
// when the SYS WIFI Provisioning module in wait for client request
}Remarks
None