1.5.3.13 SYS_WIFIPROV_Initialize Function
C
SYS_MODULE_OBJ SYS_WIFIPROV_Initialize ( SYS_WIFIPROV_CONFIG *config, SYS_WIFIPROV_CALLBACK callback, void *cookie )
Summary
Initializes the System Wi-Fi Provisioning module.
Description
Wi-Fi Provisioning service supports only single instance.
Parameters
| Param | Description |
|---|---|
| config | Wi-Fi Provisioning device configuration structure. |
| callback | The client callback function pointer. |
| cookie | The pointer which will be passed to the client application when the client callback function is invoked. |
Returns
If successful, returns a valid handle to an object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.
Example
#define WIFI_DEV_SSID "DEMO_AP" #define WIFI_DEV_PSK "password" SYS_WIFIPROV_CONFIG wifiProvConfig; SYS_MODULE_OBJ wifiProvServHandle; // Set mode as STA wifiProvConfig.mode = SYS_WIFI_STA; // Disable saving wifi configuration wifiProvConfig.saveConfig = false; //Set the auth type to SYS_WIFI_WPA2 wifiProvConfig.staConfig.authType = SYS_WIFI_WPA2; // Enable all the channels(0) wifiProvConfig.staConfig.channel = 0; // Device doesn't wait for user request. wifiProvConfig.staConfig.autoConnect = 1; // Set SSID memcpy(wifiProvConfig.staConfig.ssid,WIFI_DEV_SSID,sizeof(WIFI_DEV_SSID)); // Set PSK memcpy(wifiProvConfig.staConfig.psk,WIFI_DEV_PSK,sizeof(WIFI_DEV_PSK)); wifiProvServHandle = SYS_WIFIPROV_Initialize(&wifiProvConfig, WiFiProvServCallback, 0); if (wifiProvServHandle == SYS_MODULE_OBJ_INVALID) { // Handle error }
Remarks
Client can auto enable the Provisioning service functionality by selecting MHC configuration option of Wi-Fi Service.