1.5.3.11 SYS_WIFIPROV_Deinitialize Function
C
SYS_WIFIPROV_RESULT SYS_WIFIPROV_Deinitialize (SYS_MODULE_OBJ object)
Summary
Deinitializes the module instance of the SYS WIFIPROV module
Description
This function deinitializes the module instance disabling its operation. Resets all of the internal data structures and fields to the default settings.
Precondition
The SYS_WIFIPROV_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | SYS WIFIPROV object handle, returned from SYS_WIFIPROV_Initialize |
Returns
return SYS_WIFIPROV_RESULT
Example
if (SYS_WIFI_SUCCESS == SYS_WIFIPROV_Deinitialize (wifiProvServHandle))
{
// when the SYS WIFI is De-initialized.
}Remarks
Deinitialize should be called if the WiFi Provisioning service is no longer going to be used.