7.1.2 SET

Used to set parameters on the tool.

For lists of valid get/set parameters, see SET/GET Parameters.

Table 7-3. Set
FieldSizeDescription
SET (0x01)1 byteCommand ID
Version (0x00)1 byteCommand version
Set context1 byteContext of the parameter to set
Address1 byteParameter ID/start address
Bytes1 byteNumber of bytes to write
DataN bytesData to write

Responses:

Note: Setting multiple parameters in one set call can only be done when all fields are in the same context.