Configure the ADC
- Create a module software instance structure for the ADC module to store the ADC driver state while it is in use.
structadc_module adc_instance;Note: This should never go out of scope as long as the module is in use. In most cases, this should be global. - Configure the ADC module.
- Create an ADC module configuration struct, which can be filled out to adjust the configuration of a physical ADC peripheral.
structadc_config config_adc; - Initialize the ADC configuration struct with the module's default values.
adc_get_config_defaults(&config_adc);Note: This should always be performed before using the configuration struct to ensure that all values are initialized to known default settings. - Set extra configurations.
#if !(SAML21)#if !(SAMC21)config_adc.gain_factor = ADC_GAIN_FACTOR_DIV2;#endifconfig_adc.resolution = ADC_RESOLUTION_10BIT;#endifconfig_adc.clock_prescaler = ADC_CLOCK_PRESCALER_DIV16;config_adc.reference = ADC_REFERENCE_INTVCC1;config_adc.positive_input = ADC_POSITIVE_INPUT_PIN4;config_adc.freerunning =true;config_adc.left_adjust =false; - Set ADC configurations.
#if (SAMC21)adc_init(&adc_instance, ADC1, &config_adc);#elseadc_init(&adc_instance, ADC, &config_adc);#endif - Enable the ADC module so that conversions can be made.
adc_enable(&adc_instance);