9.6.4.2.2 Function extint_chan_set_config()
Writes an External Interrupt channel configuration to the hardware module.
void extint_chan_set_config( const uint8_t channel, const struct extint_chan_conf *const config)
Writes out a given configuration of an External Interrupt channel configuration to the hardware module. If the channel is already configured, the new configuration will replace the existing one.
| Data direction | Parameter name | Description |
|---|---|---|
[in] | channel |
External Interrupt channel to configure |
[in] | config |
Configuration settings for the channel |