25.6.4.5.2 Function tcc_set_count_value()
Sets count value for the given TCC module.
enum status_code tcc_set_count_value( const struct tcc_module *const module_inst, const uint32_t count)
Sets the timer count value of an initialized TCC module. The specified TCC module can remain running or stopped.
| Data direction | Parameter name | Description |
|---|---|---|
|
[in] |
module_inst |
Pointer to the software module instance struct |
|
[in] |
count |
New timer count value to set |
Returns
Status which indicates whether the new value is set.
| Return value | Description |
|---|---|
|
STATUS_OK |
The timer count was updated successfully |
|
STATUS_ERR_INVALID_ARG |
An invalid timer counter size was specified |