25.6.4.8.2 Function tcc_set_compare_value()
Sets a TCC module compare value.
enum status_code tcc_set_compare_value( const struct tcc_module *const module_inst, const enum tcc_match_capture_channel channel_index, const uint32_t compare)
Writes a compare value to the given TCC module compare/capture channel.
If double buffering is enabled it always write to the buffer register. The value will then be updated immediately by calling tcc_force_double_buffer_update(), or be updated when the lock update bit is cleared and the UPDATE condition happen.
| Data direction | Parameter name | Description |
|---|---|---|
|
[in] |
module_inst |
Pointer to the software module instance struct |
|
[in] |
channel_index |
Index of the compare channel to write to |
|
[in] |
compare |
New compare value to set |
Returns
Status of the compare update procedure.
| Return value | Description |
|---|---|
|
STATUS_OK |
The compare value was updated successfully |
|
STATUS_ERR_INVALID_ARG |
An invalid channel index was supplied or compare value exceed resolution |