25.6.4.1.2 Function tcc_get_config_defaults()
Initializes config with predefined default values.
void tcc_get_config_defaults( struct tcc_config *const config, Tcc *const hw)
This function will initialize a given TCC configuration structure to a set of known default values. This function should be called on any new instance of the configuration structures before being modified by the user application.
Don't run in standby
When setting top,compare or pattern by API, do double buffering write
- The base timer/counter configurations:
GCLK generator 0 clock source
No prescaler
GCLK reload action
Count upward
Don't perform one-shot operations
Counter starts on 0
Period/top value set to maximum
- The match/capture configurations:
All Capture compare channel value set to 0
No capture enabled (all channels use compare function)
Normal frequency wave generation
Waveform generation polarity set to 0
Don't perform ramp on waveform
- The waveform extension configurations:
No recoverable fault is enabled, fault actions are disabled, filter is set to 0
No non-recoverable fault state output is enabled and filter is 0
No inversion of waveform output
No channel output enabled
No PWM pin output enabled
Pin and MUX configuration not set
| Data direction | Parameter name | Description |
|---|---|---|
[out] | config |
Pointer to a TCC module configuration structure to set |
[in] | hw |
Pointer to the TCC hardware module |