4.6 Dedicated I/O Bank Pins

JTAG, SPI, and DEVRST_N signals share the same bank 3 supply and are not directly available to the fabric. SPI I/O are, however, dynamically switched over to be used by the fabric whenever the RT PolarFire controller is not using them. Dedicated I/O bank supplies must be powered up above their operational threshold and enabled before the RT PolarFire controller negates the main power-on reset to the FPGA fabric. The following tables list the JTAG, SPI, and DEVRST_N pin names and descriptions. Libero configures unused user I/O as input buffer disabled, output buffer tri-stated with weak pull-up. For more information about unused conditions, see RT PolarFire FPGA Board Design User Guide.

The JTAG bank voltages can be set to operate at 1.8V, 2.5V, or 3.3V. The following table lists the JTAG pins.

Table 4-6. JTAG Pins
Pin NamesDirectionWeak Pull-Up/Unused ConditionDescription
TMSInputYes/DNCJTAG test mode select
TRSTBInputYesJTAG test reset. Must be held low during device operation
TDIInputYes/DNCJTAG test data in

In ATPG or test mode, when using a 4-bit tdi bus, this I/O is used as tdi[0].

TCKInputNoJTAG test clock
TDOOutputNo/DNCJTAG test data out
Important: If FPGA is in System Controller Suspend Mode and TRSTB is unused, either an external 1 kΩ pull-down resistor should be connected to TRSTB to override the weak internal pull-up, or TRSTB should be driven low from the external source.
Important: In unused condition, TCK must be connected to VSS through 10 kΩ resistor.
Table 4-7. Device Reset Pins
NameDirectionWeak Pull-upDescription
DEVRST_NInput22 KΩDevice reset (asserted low).
Table 4-8. SPI Interface Pins
NameDirectionDescription
SCKBi-directionalSPI clock
SSBi-directionalSPI target select
SDIInputSDI input for the shared SPI interface.
SDOOutputSDO output for the shared SPI interface.
SPI_ENInputPulled up or down through a resistor or driven dynamically from an external source to enable or tri-state the SPI I/O.
IO_CFG_INTFInputPulled up or down through a resistor or driven dynamically from an external source to indicate whether the shared SPI interface is an initiator or a target. Dedicated to the system controller.

0: SPI target interface

1: SPI ​initiator interface

Table 4-9. Special Pins
NameDirectionDescriptionUnused Condition
NC—No connect pin. This pin indicates that it is not connected within the circuitry. NC pins can be driven by any voltage or can be left floating with no effect on the operation of the device.—
DNC—Do not connect pin. DNC pins must not be connected to any signals on the PCB, and they must be left unconnected.—
LPRB_AOutputSpecifies an internal signal for probing (oscilloscope-like feature). The two live probe I/O cells function as either of the following:
  • Live probe
  • User I/O (GPIO)
Libero-defined DNC
LPRB_BOutputLibero-defined DNC
FF_EXIT_NInputReserved—
Shield SignalOutputShield signal is required for each DDR data byte signal. It must be driven with maximum drive strength to improve the signal integrity.Only when DDR controller is in use