2.62.6 LEDx_HighDelaySet Function
C
/* x = LED peripheral instance number */
void LEDx_HighDelaySet(uint16_t hd)
Summary
Specifies the number of PWM periods to wait before updating the current duty cycle when the current duty cycle is greater than or equal to the value MAX in register LED_LIMIT
Description
Specifies the number of PWM periods to wait before updating the current duty cycle when the current duty cycle is greater than or equal to the value MAX in register LED_LIMIT
Precondition
None
Parameters
| Param | Description |
|---|---|
| hd | high delay value |
Returns
None
Example
LED0_HighDelaySet(10);
Remarks
None