2.62.5 LEDx_DutyCycleMinSet Function
C
/* x = LED peripheral instance number */
void LEDx_DutyCycleMinSet(uint8_t min)
Summary
Specifies the minimum duty cycle value.
Description
When the current duty cycle is less than or equal to the min value the breathing apparatus holds the current duty cycle for the period specified by the field LD in register LED_DELAY
Precondition
None
Parameters
| Param | Description |
|---|---|
| min | Minimum value of the duty cycle in LED breathing mode |
Returns
None
Example
LED0_DutyCycleMinSet(50);
Remarks
None