2.62.7 LEDx_LowDelaySet Function
C
/* x = LED peripheral instance number */
void LEDx_LowDelaySet(uint16_t ld)
Summary
Specifies the number of PWM periods to wait before updating the current duty cycle when the current duty cycle is greater than or equal to the value MIN in register LED_LIMIT
Description
Specifies the number of PWM periods to wait before updating the current duty cycle when the current duty cycle is greater than or equal to the value MIN in register LED_LIMIT
Precondition
None
Parameters
| Param | Description |
|---|---|
| ld | low delay value |
Returns
None
Example
LED0_LowDelaySet(10);
Remarks
None