2.62.9 LEDx_SegmentsStepSizeSet Function
C
/* x = LED peripheral instance number */
void LEDx_SegmentsStepSizeSet(uint32_t stepSzVal)
Summary
Configures the amount the current duty cycle is adjusted at the end of every PWM period
Description
Configures the amount the current duty cycle is adjusted at the end of every PWM period
Precondition
None
Parameters
| Param | Description |
|---|---|
| stepSzVal | Step size value, bitwise OR of all the steps |
Returns
None
Example
LED0_SegmentsStepSizeSet(0x87654321);
Remarks
None