2.18.10 CMPx_DACDataHighWrite Function
C
// x is the instance number of the CMP peripheral
inline static void CMPx_DACDataHighWrite(uint16_t dacHighLimit);
Summary
Sets the higher limit of slope .
Description
This inline function writes higher limit of the slope.
Precondition
None.
Parameters
| Param | Description |
| dacHighLimit | higher limit of slope |
Returns
None.
Example
CMP1_DACDataHighWrite(0xF32);
Remarks
Available only in slope mode.