2.75.9 OPAx_OutputMonitorEnable Function
C
/* x = OPA instance number */
inline static void OPAx_OutputMonitorEnable( bool enable );
Summary
Enables/disables the output of OPAx module to ADC of the device.
Description
This inline function sets or clears the output monitor enable bit for the OPAx module based on the input parameter.
Precondition
Ensure that the OPAx module is properly initialized before configuring the output monitor.
Parameters
| Param | Description |
| enable | If true, enables the output monitor. If false, disables the output monitor. |
Returns
None.
Example
OPA1_OutputMonitorEnable(true); //enabled
OPA1_OutputMonitorEnable(false); //disabled
Remarks
None.