2.75.2 OPAx_DifferentialInputModeSet Function
C
/* x = OPA instance number */
inline static void OPAx_DifferentialInputModeSet(OPA_DIFFERENTIAL_INPUT_MODE input);
Summary
Sets the differential input mode for the OPAx module of the device.
Description
This function configures the differential input mode for the OPAx module by setting the appropriate bits in the control register.
Precondition
Ensure that the OPAx module is properly initialized before configuring the differential input mode.
Parameters
| Param | Description |
| input | The selected differential input mode. This parameter should be of type OPA_DIFFERENTIAL_INPUT_MODE |
Returns
None.
Example
// Set the OPA module to differential input mode OPA_DiffInputMode mode = OPA_DIFF_INPUT_MODE_DIFFERENTIAL; OPA_SetDiffInputMode(mode);
Remarks
None.