2.31.1 DMA_Initialize Function
C
void DMA_Initialize( void )
Summary
Initializes the DMA controller of the device.
Description
This function initializes the DMA controller of the device as configured by the user from within the DMA manager of MCC.
Precondition
The DMA module clock requirements should have been configured in the MCC Clock Manager utility.
Parameters
None.
Returns
None.
Example
DMA_Initialize();
Remarks
None