2.31.5 DMA_ChannelDisable Function
C
void DMA_ChannelDisable ( DMA_CHANNEL channel )
Summary
The function disables the specified DMA channel.
Description
The function disables the specified DMA channel. Once disabled, the channel will ignore triggers and will not transfer data till the next time a DMA_ChannelTransfer function is called. If there is a transfer already in progress, this will suspended.
Precondition
DMA should have been initialized by calling DMA_Initialize.
Parameters
| Param | Description |
|---|---|
| channel | The DMA channel that needs to be disabled |
Returns
None.
Example
// Disable the channel.
DMA_ChannelDisable (DMA_CHANNEL_0);
Remarks
None.