5.6 Dual Partition Flash Configuration
For dsPIC33CK1024MP710 devices operating in Dual Partition Flash Program Memory modes, the Inactive Partition can be erased and programmed without stalling the processor. The same programming algorithms are used for programming and erasing the Flash in the Inactive Partition, as described in RTSP Operation. On top of the page erase option, the entire Flash memory of the Inactive Partition can be erased by configuring the NVMOP[3:0] bits in the NVMCON register.
Note: The application software to be loaded into the Inactive Partition will have the
address of the Active Partition. The bootloader firmware will need to offset the address
by 0x400000 in order to write to the Inactive Partition.