32.2.7 ADC Conversion Procedure (Basic Mode)
This is an example procedure for using the ADC to perform an Analog-to-Digital Conversion:
- Configure Port:
- Disable pin output driver (Refer to the TRISx register)
- Configure pin as analog (Refer to the ANSELx register)
- Configure the ADC module:
- Select the ADC conversion clock
- Configure voltage reference
- Select the ADC input channel (precharge + acquisition)
- Turn on the ADC module
- Configure the ADC interrupt (optional):
- Clear the ADC interrupt flag
- Enable the ADC interrupt
- Enable the peripheral interrupt (PIE bit)
- Enable the global interrupt (GIE bit) (see the Note 1 below)
- If ADACQ =
0, software must wait the required acquisition time (see the Note 2 below). - Start conversion by setting the GO bit.
- Wait for the ADC conversion to complete by one of the
following:
- Polling the GO bit
- Polling the ADIF bit
- Waiting for the ADC interrupt (interrupts enabled)
- Read the ADC result.
- Clear the ADC interrupt flag (required if interrupt is enabled).
Important:
- The global interrupt can be disabled if the user is attempting to wake up from Sleep and resume in-line code execution.
- Refer to the “ADC Acquisition Requirements” section.
ADC Conversion (assembly)
; This code block configures the ADC for polling, VDD and VSS references,
; FRC oscillator, and AN0 input.
; Conversion start & polling for completion are included.
;
BANKSEL ADCON1 ;
movlw B’11110000’ ;Right justify, FRC oscillator
movwf ADCON1 ;Vdd and Vss Vref
BANKSEL TRISA ;
bsf TRISA,0 ;Set RA0 to input
BANKSEL ANSEL ;
bsf ANSEL,0 ;Set RA0 to analog
BANKSEL ADCON0 ;
movlw B’00000001’ ;Select channel AN0
movwf ADCON0 ;Turn ADC On
call SampleTime ;Acquisiton delay
bsf ADCON0,ADGO ;Start conversion
btfsc ADCON0,ADGO ;Is conversion done?
goto $-1 ;No, test again
BANKSEL ADRESH ;
movf ADRESH,W ;Read upper 2 bits
movwf RESULTHI ;store in GPR space
movf ADRESL,W ;Read lower 8 bits
movwf RESULTLO ;Store in GPR space
ADC Conversion (C)
/*This code block configures the ADC for polling, VDD and VSS references, FRC
oscillator and AN0 input.
Conversion start & polling for completion are included.
*/
void main() {
//System Initialize
initializeSystem();
//Setup ADC
ADCON0bits.FM = 1; //right justify
ADCON0bits.CS = 1; //FRC Clock
ADPCH = 0x00; //RA0 is Analog channel
TRISAbits.TRISA0 = 1; //Set RA0 to input
ANSELAbits.ANSELA0 = 1; //Set RA0 to analog
ADCON0bits.ON = 1; //Turn ADC On
while (1) {
ADCON0bits.GO = 1; //Start conversion
while (ADCON0bits.GO); //Wait for conversion done
resultHigh = ADRESH; //Read result
resultLow = ADRESL; //Read result
}
}