6.6.3 NVMCON1
Note:
- Bit is undefined while WR =
1(during the EEPROM write operation it may be ‘0’ or ‘1’). - Bit must be cleared by software; hardware will not clear this bit.
- Bit may be written to
‘
1’ by the user to implement test sequences. - This bit can only be set by following the sequence described in the “NVM Unlock Sequence” section.
- Operations are self-timed and the WR bit is cleared by hardware when complete.
- Once a write operation is initiated, setting this bit to zero will have no effect.
- Reading from EEPROM loads only NVMDATL.
| Name: | NVMCON1 |
| Address: | 0x81E |
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| NVMREGS | LWLO | FREE | WRERR | WREN | WR | RD | |||
| Access | R/W | R/W | R/S/HC | R/W/HS | R/W | R/S/HC | R/S/HC | ||
| Reset | 0 | 0 | 0 | x | 0 | 0 | 0 |
Bit 6 – NVMREGS NVM Region Selection bit
| Value | Description |
|---|---|
1 |
Access EEPROM, DIA, DCI, Configuration, User ID and Device ID Registers |
0 |
Access Program Flash Memory |
Bit 5 – LWLO Load Write Latches Only bit
| Value | Name | Description |
|---|---|---|
1 |
When FREE =
0 |
The next WR command updates the write latch for this word within the row; no memory operation is initiated |
0 |
When FREE =
0 |
The next WR command writes data or erases |
| - | Otherwise: | This bit is ignored |
Bit 4 – FREE Program Flash Memory Erase Enable bit
| Value | Description |
|---|---|
1 |
Performs an erase operation with the next WR command; the 32-word pseudo-row containing the indicated address is erased (to all 1s) to prepare for writing |
0 |
The next WR command writes without erasing |
Bit 3 – WRERR
| Reset States: |
|
| Value | Description |
|---|---|
1 |
A write operation was interrupted by a Reset, interrupted Unlock sequence, or WR was written to one while NVMADR points to a write-protected address |
0 |
All write operations have completed normally |
Bit 2 – WREN Program/Erase Enable bit
| Value | Description |
|---|---|
1 |
Allows program/erase cycles |
0 |
Inhibits programming/erasing of program Flash |
Bit 1 – WR Write Control bit(4,5,6)
| Value | Name | Description |
|---|---|---|
1 |
When NVMREG:NVMADR points to a Program Flash Memory location: | Initiates the operation indicated by table in the “WRERR Bit” section |
0 |
When NVMREG:NVMADR points to a Program Flash Memory location: | NVM program/erase operation is complete and inactive |
1 |
When NVMREG:NVMADR points to an EEPROM location: | Initiates an erase/program cycle at the corresponding EEPROM location |
0 |
When NVMREG:NVMADR points to an EEPROM location: | NVM program/erase operation is complete and inactive |
Bit 0 – RD Read Control bit(7)
| Value | Description |
|---|---|
1 |
Initiates a read at address = NVMADR1, and loads data to NVMDAT Read takes one instruction cycle and the bit is cleared when the operation is complete. The bit can only be set (not cleared) in software. |
0 |
NVM read operation is complete and inactive |