3.2.4 Mi-V Processor Subsystem
(Ask a Question)The Mi-V processor subsystem configures Core10GMAC and CoreUSXGMII through Advanced High-performance Bus-Advanced Peripheral Bus (AHB-APB) interface. It also communicates with external AQR107 PHY through CoreGPIO which provides the MDIO clause 45 interface implemented in the firmware.
MIV_RV32IMA_L1_AHB Configurator sets the Reset Vector Address to 0x80000000, as shown in the preceding figure. This is the address which the processor starts executing after a reset. The processor's main memory must be accessible to Mi-V AHB memory interface whose memory-mapped address ranges from 0x80000000 to 0x8FFFFFFF. The Mi-V memory interface supports cached transactions, whereas Mi-V MMIO interface does not support them.
Mi-V subsystem communicates to the IP block using the following interfaces:
- Core10GMAC: . The following table lists the registers configured by Mi-V subsystem.
Table 3-2. Core10GMAC Registers Register Address Offset Bit Binary value MAC TX Config Register (0xA) 0x3 cfg_sys_mac_tx_en 1 0x4 sys_mac_tx_fcs_ins 1 MAC RX Config Register (0xB) 0x0 mac_rx_fcs_remove 1 0x3 cfg_sys_mac_rx-en 1 - CoreUSXGMII: . Registers configured by Mi-V subsystem are listed in the following table.
Table 3-3. CoreUSXGMII Registers Register Offset Description USXGMII-CONTROL_REG 0x0 Control: Enables/Disables the USXGMII Auto negotiation function USXGMII_STATUS_REG 0x4 Status: Indicates the link status along with auto negotiation status USXGMII_AN_ADV 0x8 Auto Negotiation Advertise: Configures the mode of operation and configures the speed selection USXGMII_AN_LP_ADV 0xC Auto Negotiation Link Partner Base Page Ability: Read Only register indicates the link partners USXGMII configuration - CoreUARTAPB: .
- Aquantia PHY (AQR107): . The following table lists the registers configured by Mi-V subsystem.
Table 3-4. PHY Registers Register Offset Description PHY REGISTER 0x4 Enables/Disables/re-start Auto Negotiation Note: For information about the features and registers of Aquantia PHY, see AQR107 Handbook. - PF_SRAM: The PolarFire system controller initializes the LSRAMs with user application and releases the system reset.