4.11 ATWILC Linux Release v15.3
The following are the new features in ATWILC Linux Release v15.3:
- Reed IQ imbalance calibration data from Efuse.
- Dynamically add network interfaces for ATWILC driver.
- Add optional rtc_clk property to dts and use it in the driver.
The following are the bug fixes for ATWILC Linux release v15.3
- Apply feedback comments from staging community to the driver.
- Fix for CF-End packets on air when multiple WILC stations are connected to the same AP.
- Fix crack Attack failure – Upgrade wpa_supplicant on buildroot to 2.7 and latest security fixes.
- Fix memory leak when connecting/disconnecting to AP continuously.
- Fix for Passive scanning feature.
- Avoid controlling power save state from the driver while obtaining IP and scanning.
- FW crash when switching between AP via link loss.
- Fix for low Tx power when using CW Tone in the Ch/C GUI tool.
- Clear pending interrupts while initializing/de-initializing the device.
- WILC3000 Low Rx performance with 11n rates.