4.12 ATWILC Linux Release v15.2
The following are the bug fixes for ATWILC Linux release v15.2.
- Regression in v15.1 while connecting to WPA AP.
- Fix for corrupted packets reported on the Monitor mode.
- Better consistency to find ATWILC softAP’s in stations' scan results.
- Consistent assignment of printed MAC address to wlan0.
- Better TX performance with significant temperature changes.
- SoftAP fails to operate correctly when its MAC address is assigned from the host.
- Staging review fixes.
- GPIO descriptor related changes. Requires changes on the host’s Device Tree file.
- Fix for crash from v15.1 when switching between AP and station interface.
- Enable Antenna diversity using GPIO3 for ATWILC3000.
- SoftAP fails to associate eigth station.
- Improve transmission performance in noisy environment.
- Fix regression causing degradation in BLE RX Sensitivity.
- Fix for ATWILC firmware overwriting MAC address in received broadcast packets.
- Incorrect pointer passed while
getting
IF handler. - Refactor
coreconfigurator.cfile to use API's provided in kernel framework. - High latency on receiving firmware start interrupt and intermittent lower throughput on SAMA5D4 board.
- iPhone intermittently fails to connect to ATWILC SoftAP.