2.3.2.2 ASPM L1 Capability
By default, the ASPM L1 Capability is enabled. Configure the settings for ASPM L1 as follows:
- L1 Acceptable Latency—Displays the list to choose one of the of following for latency values:
- Maximum of 1 µs
- Maximum of 2 µs
- Maximum of 4 µs
- Maximum of 8 µs
- Maximum of 16 µs
- Maximum of 32 µs
- Maximum of 64 µs
- No Limit
- L1 Exit Latency Separate Clock/Common Clock Mode—Displays the list to choose one of the following for the exit latency value:
- Less than 1 µs
- 1 µs to less than 2 µs
- 2 µs to less than 4 µs
- 4 µs to less than 8 µs
- 8 µs to less than 16 µs
- 16 µs to less than 32 µs
- 32 µs to 64 µs
- More than 64 µs
Note: The exit latency value you choose for the Common Clock mode must be smaller than the value of Separate Clock mode.