5.12.2 Conflict Resolution in Designer Blocks

If you instantiate more than one block in your design, you may have a conflict between the blocks. Designer manages conflicts between blocks according to the following priority:

  1. CDB file order (as specified in the CDB File Organization dialog box in the Project Manager). You can change this order in Designer; to do so, from the File menu, choose Import Source Files.
  2. Compile options set to resolve place-and-route conflicts between blocks (see below for a full explanation of the Block Instantiation compile options).
  3. PDC options set_block_options and move_block).

You can review the results of the conflict resolution in the Compile report and in the Block tab in MVN.