20.4.47.1 Arguments
-mode{value}
Selects the mode to which apply the operating condition settings. You can select a pre-defined mode or any custom mode in your design.
-best{value}
Specifies the best temperature (in degrees Celsius) for the selected mode.
-typical{value}
Specifies the typical temperature (in degrees Celsius) for the selected mode.
-worst{value}
Specifies the worst temperature (in degrees Celsius) for the selected mode.
-thermal_mode{value}
Specifies the mode in which the junction temperature is computed. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
ambient | The junction temperature will be iteratively computed with total static power |
opcond | The junction temperature will be given as one of the operating condition range values specified in the device selection |