20.4.8.1 Arguments

-pin_name {pin_name}

Specifies the name of the pin to add to the domain.

-pin_type {value}

Specifies the type of the pin to add. The following table shows the acceptable values for this argument:

Value

Description

clock

The pin to add is a clock pin

Value

Description

data

The pin to add is a data pin

-domain_name {domain_name}

Specifies the name of the domain in which to add the specified pin.

-domain_type {value}

Specifies the type of domain in which to add the specified pin. The following table shows the acceptable values for this argument:

Value

Description

clock

The domain is a clock domain

set

The domain is a set domain