9.19.2 Analog System Not Working as Expected

If the Analog System is not working correctly, it may be due the following:

  1. System supply issue.
    To troubleshoot:
    • Physically verify that all the supplies are properly connected to the device and they are at the proper level. Then confirm by running the Device Status.
    • Physically verify that the relevant channels are correctly connected to the device.
  2. Analog system is not properly configured. You can confirm this by examining the Analog System.