3.15.3 View menu
| Command | Icon | Shortcut | Function |
|---|---|---|---|
| Zoom Area |
| Drag out an area to enlarge | |
| Zoom In |
| + | Magnifies the view by a factor of 2 (scale = 2x) |
| Zoom Out |
| - | Reduces the view by a factor of 2 (scale = .5x) |
| Fit in Window |
| CTRL + W | Fits the entire design within the ChipView window |
| Redraw | F2 | Redraws the design in the ChipView window | |
| Mark | CTRL + G | Sets a pointer to the current cursor location, which you can return to by choosing Go to Mark | |
| Go to Mark | CTRL + H | Moves the cursor to your last marked location | |
| Configure List Boxes... |
| Displays the Configure List Boxes dialog box, in which you can filter which macros appear in the Assigned and Unassigned list boxes | |
| Color Manager | Displays the Color Manager dialog box, in which you set the default highlight colors for nets, clusters, and super clusters in the ChipView window | ||
| Static Objects > Cluster | Highlights clusters in their default highlight color | ||
| Static Objects > Super Cluster | Highlights super clusters in their default highlight color | ||
| I/O Banks | Not used | ||
| Toolbar | Hides or displays the toolbar buttons | ||
| Assigned List Box | Hides or displays the Assigned List Box | ||
| Unassigned List Box | Hides or displays the Unassigned List Box | ||
| World View | Hides or displays the World View window | ||
| Status bar | Hides or displays the status bar |