20.4.31.1 Arguments
-pin_name {pin_name}
Specifies the name of the pin to remove from the domain.
-pin_type {value}
Specifies the type of the pin to remove. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
clock | The pin to remove is a clock pin |
data | The pinto remove is a data pin |
-domain_name {domain_name}
Specifies the name of the domain from which to remove the pin.
-domain_type {value}
Specifies the type of domain from which the pin is being removed. The following table shows the acceptable values for this argument:
Value | Description |
|---|---|
clock | The domain is a clock domain |
set | The domain is a set domain |