20.4.5.1 Arguments
-type power_scenario
Specifies the type of report to generate is a scenario power report.
-powerunit {value}
Specifies the unit in which power is set. The following table shows the acceptable values for this argument:
|
Value |
Description |
|---|---|
|
W |
The power unit is set to watts |
|
mW |
The power unit is set to milliwatts |
|
uW |
The power unit is set to microwatts |
-frequnit {value}
Specifies the unit in which frequency is set. The following table shows the acceptable values for this argument:
|
Value |
Description |
|---|---|
|
Hz |
The frequency unit is set to hertz |
|
kHz |
The frequency unit is set to kilohertz |
|
MHz |
The frequency unit is set to megahertz |
-toggle {value}
Specifies the toggle. The following table shows the acceptable values for this argument:
|
Value |
Description |
|---|---|
|
true |
The toggle is set to true |
|
Value |
Description |
|---|---|
|
false |
The toggle is set to false |
-scenario{value}
Specifies a scenario that the report is generated from.
-style {value}
Specifies the format in which the report will be exported. The following table shows the acceptable values for this argument:
|
Value |
Description |
|---|---|
|
Text |
The report will be exported as Text file |
|
CSV |
The report will be exported as CSV file |
-battery_life {value}
Specifies whether to include the battery life summary in the report. The following table shows the acceptable values for this argument:
|
Value |
Description |
|---|---|
|
true |
Includes the battery life summary in the report |
|
false |
Does not include the battery life summary in the report |
-battery_capacity {value}
Specifies the battery capacity in A*H.
-rail_breakdown {value}
Specifies whether to include the breakdown by rail summary in the report. The following table shows the acceptable values for this argument:
|
Value |
Description |
|---|---|
|
true |
Includes the breakdown by rail summary in the report |
|
false |
Does not include the breakdown by rail summary in the report. This is the default value. |
-type_breakdown {value}
Specifies whether to include the breakdown by type summary in the report. The following table shows the acceptable values for this argument:
|
Value |
Description |
|---|---|
|
true |
Includes the breakdown by type summary in the report |
|
false |
Does not include the breakdown by type summary in the report. This is the default value. |
-mode_breakdown {value}
Specifies whether to include a breakdown by mode in the report. The following table shows the acceptable values for this argument:
|
Value |
Description |
|---|---|
|
true |
Includes the breakdown by mode in the report |
|
false |
Does not include the breakdown by mode in the report. This is the default value. |
-opcond_summary {value}
Specifies whether to include the operating conditions summary in the report. The following table shows the acceptable values for this argument:
|
Value |
Description |
|---|---|
|
true |
Includes the operating conditions summary in the report |
|
false |
Does not include the operating conditions summary in the report |
{filename.rpt}
Specifies the name of the report.