20.4.33.1 Arguments

-from {value}

This specifies the if the VCD is removed for a specific mode or for the entire project. The following table shows the acceptable values for this argument:

Value

Description

mode

The VCD file is removed for a mode

project

The VCD file is removed from the project

-mode {value}

This specifies the name of the mode for which the VCD will be removed

-filename

This specifies the name of the VCD file to be removed