9.20.3 How do I generate diagnostic reports for my target device?

A set of diagnostic reports can be generated for your target device depending on which silicon feature you are debugging. A set of Tcl commands are available to export those reports. The following is a summary of those Tcl commands based on the silicon features.

When using the –file parameter, ensure that you use a different file name for each command so you do not overwrite the report content. If you do not specify the –file option in the Tcl, the output results will be directed to the FlashPro® log window.

For the overall device
For FlashROM
For Embedded Flash Memory (NVM)
For Analog Block

To execute the Tcl command, from the File menu choose Run Script.