9.15.9.36 Example
The following reads the FROM content on the device 'AFS600' and sets to physical mapping:
read_flashrom -name {AFS600} -mapping {physical}
read_id_code
The command reads IDCode from the device without masking any IDCode fields. This is the raw IDcode from the silicon.
Note: Being able to read the IDCode is an indication that the JTAG interface is working correctly.
read_id_code [-name {device_name}]