20.4.44.1 Arguments

-mode {value}

Specifies the mode in which the junction temperature is computed. The following table shows the acceptable values for this argument:

Value

Description

ambient

The junction temperature will be iteratively computed with total static power

opcond

The junction temperature will be given as one of the operating condition range values specified in the device selection