4.60 #undefine Directive
The MPASM #undefine directive undefines textual replacement for a
macro.
Suggested Replacement
As assembly source files can be preprocessed, the PIC Assembler's
#undef preprocessor directive can be used as a direct
replacement for this directive, as shown in the example below.
Ensure the assembly source file uses a .S extension so that it will
be preprocessed by the assembler, or alternatively, use the
-xassembler-with-cpp option to request that source files be
preprocessed regardless of their extension.
;ensure the macro has been cleared first
#ifdef SUMSP
#undef SUMSP
#endif
;now create a new macro
#define SUMSP(a, b) (a+2*b)
PSECT text,class=CODE
process:
movlw SUMSP(5, 3)
movwf volume