4.40 Macro Directive
The MPASM MACRO directive defines a macro.
Suggested Replacement
The PIC Assembler's MACRO directive is direct
replacement.
Within a macro definition, the & character can be
used to permit the concatenation of macro arguments with other text, but is removed
in the actual expansion. For example:
loadPort MACRO port, value
movlw value
movwf PORT&port
ENDM
will load PORTA if port is
A when called, etc. The special meaning of the
& token in macros implies that you must only use the
and form of the bitwise AND operator.
A comment can be suppressed within the expansion of a macro by opening the comment
with two semicolons, ;;.
When invoking a macro, the argument list must be comma-separated. If it is desired to
include a comma (or other delimiter such as a space) in an argument then angle
brackets < and > can be used to quote.
If an argument is preceded by a percent sign, %, that argument will
be evaluated as an expression and passed as a decimal number, rather than as a
string. This is useful if evaluation of the argument inside the macro body would
yield a different result.
The nul operator can be used within a macro to test a macro
argument, for example:
IF nul arg3 ;argument was not supplied.
...
ELSE ;argument was supplied
...
ENDIF