4.56 Udata Directive
The MPASM UDATA directive creates a section for objects that
are uninitialised..
Suggested Replacement
Use the predefined udata_bankn psect, where
n represents the bank number in which the psect
should reside, or a create a similar psect, ensuring the flags are suitable for a
section containing variables on the target device.
The PIC Assembler provides the udata_bankn psect
once you include . You can use this
psect without having to specify any psect flags, for example:<xc.inc>
#include <xc.inc>
PSECT udata_bank1
;data goes here
Alternatively, you can define your own psect with any name and suitable psect flags.
The psect's
space flag must be 1, to indicate that the psect should
be positioned in data memory. Typically, you would use the class
flag to assign the psect to one of the BANKN linker classes,
where N represents the bank number for which the class
defines. These classes are also predefined by the driver, so that the psect will be
positioned somewhere in the memory associated with the specified class without you
having to specify any linker options. You could also position this psect at a
particular address using the linker's -p option, passed to the
linker from the driver's -Wl option. For
example:PSECT myData,space=1,class=BANK1
;data goes here